(0)| 1/22/2025 9:16 AM | |
|
Joined: 11/12/2012 Last visit: 12/19/2025 Posts: 41 Rating:
|
Hello, is possible to use a managed switch which is not a PROFINET switch (no GSD file available) and have the topology functionlaity. This one for example: https://www.planet.com.tw/en/product/igs-6325-8up2s2x-v2 Thnaks |
| 1/22/2025 9:24 AM | |
|
Joined: 5/12/2006 Last visit: 12/19/2025 Posts: 22816 Rating:
|
no |
| 1/22/2025 2:18 PM | |
|
Joined: 7/24/2024 Last visit: 12/22/2025 Posts: 75 Rating:
|
Hi, the topology function only works with PROFINET devices, and while it is possible to load configurations with devices that are not PROFINET devices, this may result in errors. You can find more information in this FAQ: Connections shown in red in the Topology view of the TIA Portal |
This contribution was helpful to
|
|
Follow us on