(0)| 1/23/2025 9:06 AM | |
|
Joined: 7/9/2015 Last visit: 1/19/2026 Posts: 4500 Rating:
|
Hi, this order number belongs to a bundle. interface module (6ES7155-6AU02-0BN0), server module (6ES7193-6PA00-0AA0), SIMATIC bus adapter BA 2x RJ45 (6ES7193-6AR00-0AA0). Do you find this order numbers? If not: PROFINET GSD files: I/O – ET 200SPRegards, Towome |
|
|
|
| 1/23/2025 9:03 PM | |
|
Joined: 7/7/2010 Last visit: 1/22/2026 Posts: 16407 Rating:
|
This is the same information provided by the prior posts, but may be packaged in a way you can understand better.. I had no problem understanding. But, if you are new to TIA Portal and/or using non-integrated GSD/GSE/GSDML device/module files, this may help. Download this zip file from a prior post's link: https://support.industry.siemens.com/cs/attachments/57138621/ET200SP_IM155-6_Archivstaende.zip Inside that .zip are several versions of non-integrated support the 6ES7155-6AA02-0BN0 - which as stated in the device datasheet required V19+ for TIA Portal built-in integration. The one you may have immediate luck with is GSDML 2.43. However, if you can get success with a higher (newer) version GSDML file, it may work better and have less glitches or problems over time. Use the PDF linked on ( https://support.industry.siemens.com/cs/document/57138621 ) if you have problems manually integrating the device into your v16 project. Look for your device in the "Other" section (bottom of the hardware list).
|
|
science guy |
|
This contribution was helpful to
|
|
Follow us on