4/2/2024 10:28 AM | |
Joined: 10/22/2021 Last visit: 6/26/2025 Posts: 2 Rating:
|
Thanks Stefan, Where can I find this user? How do I manage his privileges? |
4/2/2024 11:41 AM | |
Joined: 1/21/2013 Last visit: 9/15/2025 Posts: 4110 Rating:
|
Hi SPSiberg, The full path for the user is "NT SERVICE\WCCILScsService". It is a hidden system user on the PC on which the WinCC Unified PC Runtime is installed. The user is a member of the groups PlcSimUsers, RTIL Tracing Users, SIMATIC HMI, umcd_domain_manager, umcd_dsso, umcd_um and UM_CONFIG. This is the information I was able to get from my computer. However, granting access to this user will be challenging, as you will usually need a local account on the computer providing the share, or a domain user. However, I cannot advise you on how to handle this. The only suggestion is to use the WriteFile method to write a new file to the share. This should be done by the same user account, and may be easier to test than database access, which may also be related to an ODBC configuration error. Kind regards |
Follow us on