4/6/2023 2:34 PM | |
Joined: 2/18/2020 Last visit: 7/28/2025 Posts: 43 Rating:
|
I'm facing a similar issue. As far as I understand from the 3.1.1 Dynamizing object properties via scripts paragraph of the SIMATIC WinCC Unified Tips and Tricks for Scripting, should be able to set the value of an IO field by the following code:
But when I start the simulation I get the error relative to the IO Field:
Any hint on how to solve this? Edit: I've just realized that I should set a trigger to run the script. Is there any way to trigger the script on page load? ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_298806 at: 04/06/2023 14:59:26Last edited by: Jen_Moderator at: 04/09/2023 06:50:36New subject after splitting |
|
4/20/2023 11:55 AM | |
Joined: 2/18/2020 Last visit: 7/28/2025 Posts: 43 Rating:
|
Yes, since I need to trigger the Script execution as a property dynamization. Is there any other/better way? |
Follow us on