2/19/2025 10:29 AM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi As from TIA V20, it is possible to improve the RT performance (e.g. for screen changes), in the case of the use of high resolution images, by using the setting “Optimize the size of high resolution raster graphics”. This applies in particular for the case of using the high resolution images in a small presentation size. TIPs:
Thanks to Sebastian Beck and the Siemens development team for the tips.:) Sample project (archived from TIA Portal as .zap20 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! AttachmentgraphicResolution_20250114_0712.zip (116 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
Follow us on