3/6/2025 11:03 AM | |
Joined: 4/23/2014 Last visit: 8/6/2025 Posts: 2 Rating:
|
Hi, Have you solved your issue? I could add from the beginning CP1543-1 because I already had the new version of CPU but I have problem with the power segment on the bus. In my situation I have two CP 1543-1 for each 1513R rack. When the CPUs are energized with two CP1543-1, the CPU are in "power fail" alarm and watching on TIA, I have the attached situation. Note: The CP 1543-1 has arrived with a little bus connector to be used behind the Processor. Thank you in advance ------------------------------------------------------------------------------------------ |
Last edited by: PiaPiazz at: 03/06/2025 11:13:32Last edited by: Moderator_Lan at: 03/06/2025 15:06:50New subject after splitting |
|
3/6/2025 3:09 PM | |
Joined: 7/30/2024 Last visit: 9/17/2025 Posts: 961 Rating:
|
Closed because the question has been posted twice. The active topic can be found here: Redundancy with 1513R. 2 CP1543-1 for each CPU rack. possible?
Kind regards, Moderator_Lan |
Follow us on