(0)| 1/30/2015 1:04 PM | |
|
Posts: 11 Rating:
|
Hello AutoGen_1005492, have a look at this manual: https://support.automation.siemens.com/WW/llisapi.dll/csfetch/102051766/ba_scalance-s_76.pdf?func=cslib.csFetch&nodeid=102051954&forcedownload=true Regards |
Last edited by: Min_Moderator at: 1/30/2015 3:31 PMChange link to permanent |
|
| 8/2/2015 9:58 AM | |
|
Posts: 1742 Rating:
|
Hello, Now You put your PC in the range of the IP address that you want to assign to the red interface of the S6xx and you connect to that interface. Than you have several possibilities to set the IP: 2) if the method above dos not work, you can use the PST (primary setup toll) found on the CD of the S602. 3) an alternative tool is proneta. Is also a free tool. 4) you could use Step7 via "Edit Ethernet node", or TIA via the device detection. Be aware that you can only assign the IP once. If you made a mistake, you must reset to factory again using the button on the back.
The web interface of the S6xx cannot be used for configuring the S6xx. The Web interface is intended for the login of users, if you have created user specific firewall rules.
|
| 4/7/2017 5:17 PM | |
|
Posts: 9 Rating:
|
|
| 4/14/2025 5:27 AM | |
|
Joined: 7/17/2024 Last visit: 12/19/2025 Posts: 8 Rating:
|
Hi John, are you able to solve this problem? Im having the same issue |
Follow us on