2/17/2025 6:06 AM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi Scyzoryk96, It is hard to say whether a feature seems right or not. However, it is what is written in the documentation. The system function cannot be used when UMC servers with central user management or remote access are used. Kind regards |
2/17/2025 12:52 PM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi Scyzoryk96, It would also be possible to change the user using the 'ChangeUser' system function. However, since this function requires a password to be specified, this would reduce security since you would have to store the password somewhere. Kind regards |
This contribution was helpful to
1 thankful Users |
4/22/2025 5:24 AM | |
Joined: 12/7/2020 Last visit: 8/28/2025 Posts: 50 Rating:
|
Hello! I changed my "Barcode Scanner Login" script to use the "ChangeUser" system function. On the server side, once again, everything works perfectly, but on the client side it doesn't work. In Trace Viewer I get the error:
I didn't transfer a client license yet; is that an issue? Thanks for the help!
|
Follow us on