5/4/2025 2:46 PM | |
Joined: 4/22/2025 Last visit: 8/26/2025 Posts: 2 Rating:
|
Hello everyone. Preface: there is a 4-axis control system based on CPU S7-315-2DP (6ES7315-2AH14-0AB0 v3.0) with a programme developed in Step 7 v5.5. From the PLC an operator panel was connected via MPI and a control unit S120 CU320(6SL3040-0MA00-0AA1 v2.6.2) configured in Starter via DP. This system is now fully operational. 'Communication' of the PLC with the S120 is performed using Telegram 111 and the functions DPRD_DAT and DPWR_DAT. Task: to migrate the PLC project to TIA Portal v17 on an updated component base: PLC - S7-315-2 PN/DP (6ES7 315-2EH14-0AB0 v3.2.6), TP700 Comfort operator panel and keep the S120 in the same state (do not change anything in the Starter project). Updated topology: PLC - operator panel - Profinet, communication with S120 - Profibus DP (X1 port of PLC MPI/DP). I completely migrated the project to a new PLC in Tia v17, created a new operator panel, but I don't understand how to be with S120. Hardware Catalog doesn't have the S120 version I need (v 2.6.2), I couldn't find the gsd file for it either (maybe I didn't look hard enough). I would like to use the S120 as an IO_Device, so that I don't have to change the settings of the servo system, which are fully functional (and I don't have this possibility, in principle, from the Tia environment). It seems to me that devices from Hardware catalogue - Other field devices/PROFIBUS DP/Drives/SIEMENS AG/SINAMICS/6SL3 040-1MA00-0xxx can meet such requirements. But there are many versions there, the youngest of which is 4.3. I can add this device to topoligy and assign the telegram type and address space, but I'm not sure if this is a workable option as at least I'm not sure of the version. Please suggest ways to solve the problem, if they exist. Please excuse my English. Thank you in advance. Sergio upd Found the gsd file on this page. https://support.industry.siemens.com/cs/us/en/view/49216293 The question has been put to rest for now. |
Last edited by: U_d4fc9939-d145-4f6a-9f8a-ad8f8adb5514 at: 05/04/2025 15:06:28Last edited by: U_d4fc9939-d145-4f6a-9f8a-ad8f8adb5514 at: 05/05/2025 05:58:58Last edited by: Moderator_Lan at: 05/05/2025 07:05:37link optimized |
|
Follow us on