6/4/2025 7:55 AM | |
Joined: 9/30/2016 Last visit: 9/17/2025 Posts: 947 Rating:
|
How / where can I see if I am using the full available power? Please also see the attached screenshots. The PLC is programmed in Simatic Manager K5.6.2.9, and drives in Starter and the HMI is programmed in TIA V18. I have been asked if the motor / drive is running at full power or not. We have trends for 4 analog values for the drive / motor - see pic 1 and pic 2 where the current is highlighted. I looked in "Show all tags) in the "PLC tags" pic 3 and pic 4 but I cannot see current, setpoint, torque or speed for the motor there. How / where can I find the values and programming / control of these 4 analog values? I also found the motor / drive current in the "Tag Managemet in WinCC" and it is located in DB2008,DD216 (see pic 5) but where is DB2008 in the PLC? How do I search for it - see pic 6? AttachmentDorndrive.zip (79 Downloads) |
Last edited by: xmnj at: 06/04/2025 10:16:13 |
|
Follow us on