(0)| 6/20/2025 2:36 PM | |
|
Joined: 3/24/2016 Last visit: 11/22/2025 Posts: 8 Rating:
|
Hi, I have a broken OSM BC08 on my network and do not have intention on replacing it by a used one because it is an obsolete part. In the file attached you can see how my network is and how i tried to manage it without the broken OSM. Tried to use two OMC TP11 as a point to point connection but it didn't work. The error LED is always lit. Would the Scalance X101-1 work in the way i tried to work with the OMC TP11? If not, what alternative do i have? Attachmentosm bc08 network.pdf (336 Downloads) |
Follow us on