(0)| 7/10/2009 8:44 AM | |
|
Joined: 5/8/2006 Last visit: 10/23/2025 Posts: 1085 Rating:
|
G'Day You have at least two possibilities: 1. Possibility You can use thedatalogs of WinCC flexible and the system function "Log Tag". If you need the actual value of a tag, then you can storethecurrent value in a archive which you can project in WInCC flexible. 2. Possibility You can create your own script in which you store all relevant tags. If you want to show the data in an trend view, then you have to save the data in the right order of an WinCC flexible archive. Maybe this FAQsis very helpful: http://support.automation.siemens.com/WW/view/de/26190516 If you have an PC, then you can use this method: http://support.automation.siemens.com/WW/view/en/35929465 Bye |
Follow us on