7/14/2025 11:08 AM | |
Joined: 7/9/2015 Last visit: 8/29/2025 Posts: 4443 Rating:
|
Hi, I think the correct fiber optic connection for the HSYNC modules (6ES7960-1CB00-0AA5) is: X3 P1 (Primary) ⟶ X3 P1 (Backup) X4 P1 (Primary) ⟶ X4 P1 (Backup) However, each pair must be connected in a crossed configuration: X3 P1 (Primary) ⟶ X3 P1 (Backup) X4 P1 (Primary) ⟶ X4 P1 (Backup) But you must also ensure that: - The fiber cables are not swapped (TX to RX and vice versa). - The fiber cables are clean and undamaged. - The HSYNC modules are properly seated and powered. Check this: SIMATIC S7-1500R/H CPU 1517H-3 PN Regards |
|
|
Follow us on