9/10/2025 12:40 PM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35955 Rating:
|
There's no HSP for TIA V16. To use the firmware V4.6 complete you need TIA V18. |
9/10/2025 12:42 PM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35955 Rating:
|
But you can use a V4.4 program also in the CPU with V4.6. |
9/10/2025 3:02 PM | |
Joined: 3/30/2020 Last visit: 9/11/2025 Posts: 35 Rating:
|
But when i try to download, TIA V16 will crash |
9/10/2025 3:40 PM | |
Joined: 3/30/2020 Last visit: 9/11/2025 Posts: 35 Rating:
|
If i stay in TIA V16 and ignore the warning but whenever i download to the PLC, TIA V16 will crash. |
9/11/2025 12:53 AM | |
Joined: 3/30/2020 Last visit: 9/11/2025 Posts: 35 Rating:
|
My Tia v16 is already updated to version 8 and also i will try to update the ALM to 6.2 |
Follow us on