9/16/2025 8:41 AM | |
Joined: 2/8/2018 Last visit: 9/16/2025 Posts: 42 Rating:
|
Hi @bergmanu, I'm working with IoT2050 Basic and I need to know the compatibility between the firmware version/image version and FS version. Where can I find this information? That's why I'm working with different IoT2050 units, wih different FS (02, 07 and 08). I have already checked this page Downloads for SIMATIC IOT20x0 - ID: 109741799 - Industry Support Siemens but it's not so clear which fw and image version can be used depending on FS version. I would like to create a "standard" version (fw+image) to use as a clone to setup all of them, to be able, at the end, to install my applciation (developed with node-red) and be sure that will work. Let me know please and thanks for the support. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/16/2025 09:50:06New subject after splitting |
|
9/18/2025 11:33 AM | |
Joined: 3/12/2024 Last visit: 9/18/2025 Posts: 187 Rating:
|
Hello FT82, please check our IOT2050 Overview in the Forum. There we mentioned a link to information about FS-states and delivered firmware versions. Your device are delivered with the mentioned firmware versions - you can then visit our Download Page and Download your correct OS version or / and update to latest firmware versions as described in our tutorials. As you are using node-red we would recommend to update your firmware versions to the latest version and to use the latest Example Image (comes with Node-Red pre-installed). Maybe you can build some kind of an bootable image with a script that checks for the current fw-version and performs an update to the latest version. But we don't have concrete experiences on this. BR |
Follow us on