(1)| 12/23/2025 9:20 AM | |
|
Joined: 1/21/2013 Last visit: 12/24/2025 Posts: 4365 Rating:
|
Hi mdarende, The "SendEmail" system function is still very new. It's possible that the developers haven't tested enough scenarios yet. Testing is more difficult because it involves communicating with an external system that has many possibilities. Nevertheless, creating a support request would be helpful. As far as I know, the "SendEmail" system function uses the email feature within the reporting control. Testing this feature in a reporting control might provide more information about the issue. Keep in mind that different user privileges apply when testing connectivity to the server. Running the Telnet command in a terminal may not produce meaningful results because the SIMATIC WinCC Unified PC Runtime runs tasks as the WCCILScsService user. Therefore, using the StartProgram system function with Telnet may be more meaningful. Kind regards |
This contribution was helpful to
|
|
Follow us on