(0)| 12/23/2025 9:31 AM | |
|
Joined: 1/21/2013 Last visit: 12/24/2025 Posts: 4365 Rating:
|
Hi rafalsky, It seems to me that the tag logging isn't working properly anymore. When the storage device is unreachable, the logger should temporarily buffer the data. However, if the buffer is exceeded, old data will be deleted. I'm not sure if this functionality existed in version 19.0.0.2, but I recommend verifying that the tag logger is running. You can use the alarm control to do so. If you don't have an active filter, a system alarm will appear if there is an issue with tag logging. As an alternative, you can use the Trace Viewer to examine the "WCCILtlg" application. Kind regards |
Follow us on