(0)| 1/20/2026 5:51 AM | |
|
Joined: 1/21/2013 Last visit: 1/20/2026 Posts: 4418 Rating:
|
Hi fsoliman355, The following information can be found in the documentation: Call of error OBs in connection with cyclic interrupt OBs The runtime of a cyclic interrupt OB must be significantly smaller than its time interval. Otherwise, it could still happen that the time interval of a cyclic interrupt has expired but the corresponding cyclic interrupt OB is still being processed. In this case, the operating system generates a time error (calls OB 80). The cyclic interrupt that caused the error is executed later or discarded. However, only one cyclic interrupt OB for each priority can be executed later. Kind regards |
This contribution was helpful to
|
|
Follow us on