(0)| 7/26/2009 4:05 AM | |
|
Joined: 1/17/2006 Last visit: 12/28/2025 Posts: 555 Rating:
|
Hello, Edr, I got your suggestion and tested it today but without success. So, when Igo to edit ethernet node > browse, I can find in the list the ET200S IM151-3 with IP 0.0.0.0 andnone in Device name, but the MAC address is found.Then, when I try to assign an IP address and the device name, one message error appears saying that this MAC address could not be found. Andwhether I go again in edit ethernet node > browse, now I can´t find the ET200S IM151-3 in the list !!! Inone moment of the test I could assign the IP address and device name without errors (I don´t know why - it seems unstable), but when rebooting it the ip address is set back to 0.0.0.0 and the the ET200S keeps giving an BF and SF error, andin the STEP7 whenI look online it says that CPU can't connect to the ET200S. I checked the cable and it is ok. I also have one RF180C in the same network (with scalance X208)and I can assign the IP address and device name to it perfectly. I found another thread in forum with the same problem, but withou solving... /tf/WW/en/Posts/22266 Can anyone help me ? Best regards, Berg |
| 7/28/2009 1:29 AM | |
|
Joined: 1/17/2006 Last visit: 12/28/2025 Posts: 555 Rating:
|
Hello, First, thank you all for the answers! I have tried your suggestions and tips, but I didn´t have success yet. I am posting here some application pictures (STEP7 printscreen)to illustrate the real situation. I followed the steps below: 1) Image1 -> ET200S was found with IP 0.0.0.0 and MAC address, pressed<OK>; 2) Image2 -> I filled the IP address and Subnet mask, pressed <Assign IP Configuation>. The error4502:686 is showed; 3) Image3 -> In the <Browse...>window I can´t find the ET200S in the list! Only if I restart (power off) the module I can find the ET200S (IM151-3PNHF), but I can´t assign IP address again. I have checked the cable again today, and it is ok. I really don´t know what to do. Maybe with these picturesI can pass to you the situation more clearly ! I hope... Best regards, Berg Attachmentim151_3PN.zip (227 Downloads) |
| 7/28/2009 9:57 AM | |
|
Posts: 25 Rating:
|
hi, Attachmentconfiguration.zip (288 Downloads) |
Follow us on