(0)| 9/18/2009 9:51 AM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hi hoang.nh.0512 ,
i don't understand what are you asking for, sorry There is not .xml file for each batch order you create in SIMATIC Bach application, but new order batch are stred inside "atch Apllication Database". When you restore data, you can restore all data like recipes and formulas and material but not batch order. Can you tell more aout your trouble regards |
| 9/18/2009 1:15 PM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hi hoang.nh.0512,
*.sbb files are cretaed with Export/Backup function (means buckup an existing project).
You have to download process cell created into simatic Manager to start to work on BCC for a new process cell. Simples step you have to perform to create & download new process cell: 1) open project into simatic manager 2) right click on project name and select SIMATIC Batch (opens Batch configurator) 3) configure station has to work on Batch 4) generate blocks type 5) compile phase 6) select project project in Batch configutaor and transfer OS (you have to do once at begi and always after complete OS compile with memory reset) 7) download process cell open BCC 8) insert authorization for Administrator lie superuser 9) ONLY now you can create first process cell in BCC and start to create your recipe/formulas/material If you installed SIMATIC Batch on your Engineering station you can look in online documentation for "SIMATIC BATCH - Configuration Started" Hope can help Regards |
| 9/21/2009 6:31 AM | |
|
Posts: 11 Rating:
|
Hi, Cbo Finally, I deal with my trouble. Thanks for your helpful support. Best Regards. |
Follow us on