(0)| 10/2/2009 11:56 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hello guys, I'm just starting with PCS7 and need a quick answer to my question. I want to automate a factory which has two PC stations and one S7-400 and some S7-300 ÇPU's. Two two PC stations are not in operation. I have a laptop with PCS7 software and I want to create the hardware configuration. I can create one ES station for one PC and a operator station for the second one. Also I have my laptop which will communicate through PG/PG to the S7-400 CPU. Now I want to create the Wincc application but I don't know how to create it. Do I have to use only a OS station, or OS(Client), or do I have to use the Wincc OS from the ES station. I don't excactly know how the layout should look like. Or do I need to use my laptop as an ES station and then if the PC's are operational, swiththe laptop for the PC?? I hope I explained it right. Thank you Best regards |
Last edited by: Oreca at: 4/17/2010 7:18 PMIf I could help you, you can use the RATE button. Thank you. |
|
| 10/5/2009 9:28 AM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hi Sandor-CRX, with PCS7 project need create into project "PC Station" how many "station do you have on the plant :WinCC server" or "WinCC appl. StBy" forRedundant server and "WinCC Client appl". 1 - on ES create PC Station in component view 2 - open PC station HW configuration to insert "WinCC appl." for OS server, or "WinCC Client appl." for WinCC client 3 - insert card comunication your OS station is equipped with, congure MAC address and IP if need 4 - in NetPro configure connection between OS and AS 5 - download HW and SW over all station (OS and AS) and comunication For detailed info have a look on manual installed with PCS7; Windows button Start -> All Program -> Simatic -> Documentation -> English -> PCS 7 - Configuration Manual Engineering System expecially chapter "7 - Configuration of the PCS 7 Engineering System" (depending from your version) Hope can help Regards |
Follow us on