(0)| 10/28/2009 2:33 PM | |
|
Joined: 5/28/2008 Last visit: 9/1/2025 Posts: 901 Rating:
|
Hello Import-User-1, create a button and set on "Click" the Event "OpenControlPanel". then you transfer the project to your panel. the panel will turn in runtime after starting. the you can click on the button an the control panel willopen. the problem you have depent on the settings for "Autostart". here you will find something to read to solfe the problem: http://support.automation.siemens.com/WW/view/en/23034454 (if you doesn´t have a chance to open the control panel, then you must reset the panel here the help for thise case: http://support.automation.siemens.com/WW/view/en/19701610) regards Manfred |
Follow us on