(0)| 12/18/2008 11:36 AM | |
|
Joined: 8/11/2006 Last visit: 12/3/2025 Posts: 29 Rating:
|
Hi guys, Ihave this problem: on my Flexible the "save as version" function is not enabled. After a brief search, I discovered that this is an option and must be activate when you install the software (/tf/WW/en/Posts/21356). I try to reinstall the software, butI don't find this field (I don't know if this choice is possible to do only the first time you install the program!). How ispossibleenable this function in a second time? I'm working with WinCC Flex 2008 + HF2 (Step7 5.4 SP4). Thank |
| 12/18/2008 2:20 PM | |
|
Posts: 1611 Rating:
|
Hi, what operatings system did you use WinXP or Vista. If you have Vista, thenyou did not have the function "Save as version"! -> http://support.automation.siemens.com/WW/view/en/29735640 (point 3.3) I have also install the option later under WinXPand it works. regards, |
| 2/25/2009 11:23 AM | |
|
Posts: 24 Rating:
|
Ok . Thanks |
| 11/5/2009 11:04 AM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Dear Micael, That is correct, see the following links: how can you save WinCC flexible projects/libraries as projects/libraries in the format of an earlier version of WinCC flexible? What are the solutions offered for working with different versions of WinCC flexible? Perhaps the option 'Pack and Go', might be useful: how can you make an indirect transfer with Pack & Go in WinCC flexible? Best regards, Wizard |
Follow us on