(0)| 11/17/2009 5:58 PM | |
|
Posts: 1611 Rating:
|
Hi, 1.) -> you should say when the script have to be "work"! There are different ways possible. a) you can usea Tag,property > events > Changevalue" b) look to the scheduler (device settings) there are differnt option which you can use. 2.) Look to this FAQ -> http://support.automation.siemens.com/WW/view/en/23842653 There are use the function "ChangeConnection". I mean this could you use too. You must evaluation when one of the plc are in "Stop".with this signal you set the event for "ChangeConnection". regards, |
Follow us on