(0)| 12/14/2009 2:45 PM | |
|
Joined: 12/9/2009 Last visit: 10/30/2025 Posts: 156 Rating:
|
Hello, in the manual "SIMATIC ET 200S Serial interface modules" do you find more information about the communication blocks FB3 "S_SEND" and FB2 "S_RCV" http://support.automation.siemens.com/WW/view/en/9260793 When the valueof the input parameter "R"onFB3 "S_SEND"is "1"thensending is disabled. Whenthe value of the input parameters "R" = 1 and/or "EN_R" = 0onFB2 "S_RCV"then receiving is disabled. Normaly with positive edge on input parameter "REQ" the send and receive job should be started. Best Regards and good luck |
Follow us on