(0)| 12/18/2009 10:45 AM | |
|
Joined: 5/28/2008 Last visit: 9/1/2025 Posts: 901 Rating:
|
Hello YogendraG, it depends on your memory card and many other things. Here a help for receipes: Calculation of memory requirements The memory space required by each recipe (in KB) is derived from the sum of D1 + D2 + D3. Valid is:
The total length of the name of the corresponding data record in all languages (max. 255 bytes per language) + overhead per data record (1 byte + number of languages * 3 bytes). D1, D2 and D3 are rounded to the next higher number. Memory requirements for using arrays The memory required by each recipe (in KB) is derived from the sum of D1 + D2 + D3. Valid is:
The total length of the name of the corresponding data record in all languages (max. 255 bytes per language) + overhead per data record (1 byte + number of languages * 3 bytes). D1, D2 and D3 are rounded to the next higher number. |
| 12/23/2009 9:13 AM | |
|
Joined: 11/9/2008 Last visit: 1/10/2026 Posts: 414 Rating:
|
Dear Manfred, Thanks for your valuble Information. I'll check with my system and then come to You. Regards, Yogendra G |
Follow us on