(0)| 1/23/2010 11:44 AM | |
|
Joined: 5/28/2008 Last visit: 9/1/2025 Posts: 901 Rating:
|
Hello SilverSand, thats no prblem. the best way is to use the actually version of WinCC flexible. So, now you have to install SP1 first. Here the Link: http://support.automation.siemens.com/WW/view/en/34778772 Second installation is HF3 for SP1. Here the Link: http://support.automation.siemens.com/WW/view/en/36540041 After installation you use the newest version of WinCC flexible. The project you projected with WinCC flexible 2008 you also could open and work with it. I hope the information will help you... regards Manfred |
Follow us on