(1)| 3/16/2010 1:28 PM | |
|
Joined: 12/9/2009 Last visit: 10/30/2025 Posts: 156 Rating:
|
Hello, it`s right to use the function blocks FC5 "AG_RECV" and FC6 "AG_RECV" from the library SIMATIC_NET_CP -> CP 300 for the S7-300. It`s also right to use the function blocks FC50 "AG_LSEND" and FC60 "AG_LRECV" from the library SIMATIC_NET_CP -> CP400 for the S7-400. I adviseyou tosave the status when the error flag comes.I thibk the state 8180 don`t comes with error flag. Under the following link you can finda sample program for: -FC5 and FC6 inclusive evaluation of status: http://support.automation.siemens.com/WW/view/en/24675522 -FC50 and FC60inclusive evaluation of status: http://support.automation.siemens.com/WW/view/en/24693800 Best regards Little Holmes |
Follow us on