(1)| 3/18/2010 9:34 AM | |
|
Joined: 8/25/2005 Last visit: 12/30/2025 Posts: 1162 Rating:
|
Hello yuvalg, maybe PROFINET will be the solution for you? Please have a look at the examples published atSIMATIC Net Quick Start Best regards Sabine |
| 3/18/2010 10:07 AM | |
|
Posts: 8 Rating:
|
Hello Hulzhex |
| 3/18/2010 11:04 AM | |
|
Joined: 12/9/2009 Last visit: 10/30/2025 Posts: 156 Rating:
|
Hello, The CP343-1EX11 supports maximum 16 S7 connections. http://support.automation.siemens.com/WW/view/en/8777308 You can use the S7-300 Station as Client station for S7 communication. It establishes the S7 connections to the IM151-8 CPUs andcollects the data from your IM151-8 CPUs with the PUT and GET function blocks. So the IM151-8 CPU acts as server for S7 connections. The CPU 317-2PN/DP supports 32 instances. That means 32 PUT/GET function blocks. With PUT/GET support max. 160Byte data transfer. With BSEND/BRECV 32kByte are possible. http://support.automation.siemens.com/WW/view/en/12996906 Another possibility open communication via Industrial Ethernet with ISO-on-TCP, TCP or UDP. Best regards Little Holmes |
This contribution was helpful to
|
|
Follow us on