(0)| 3/31/2010 11:13 AM | |
|
Joined: 12/9/2009 Last visit: 10/30/2025 Posts: 156 Rating:
|
Hello, do you want to configure the S7-200 as DP slave or DP master?In the S7-200 station you needthe modul EM 277 to connect the S7-200 as DP-slave to a PROFIBUS DP network. In the following manual you can findthe description how you can do this (chapter "Technical Data EM 277 PROFIBUS-DP module: http://support.automation.siemens.com/WW/view/en/1109582 You will need a PROFIBUS PC CP, for example CP5611 or CP5621 with SIMATIC NET PC software to configure andusea PC station as DP master or DP slave. Here you can find some guidelines to configure the PC station: -as DP master http://support.automation.siemens.com/WW/view/en/29645558 -as DP slave http://support.automation.siemens.com/WW/view/en/16650883 Best regrads Little Holmes |
Follow us on