(0)| 4/9/2010 12:33 PM | |
|
Posts: 3609 Rating:
|
Import of a Technical Question of an User Laujofa wrote: Hello, I try to make the examples from https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=12429336&caller=view (zEn26_02_TF___31xC_Cnt - PWM 1 First steps) I use to simulate the PLCSIM and VAT but the output of the block remanis in 0. The input and hardware configuration is correct. Thank you. |
| 4/10/2010 2:28 PM | |
|
Posts: 1 Rating:
|
I need some help. I download the example from this page, I folow the step presented on the manual but when I simulate whit VAT and PLCSIM the output don't change. When I change the variable of the input in VAT the input on program is update. The example is zEn26_02_TF_____31xC_Cnt, PWM first time. |
| 4/12/2010 7:57 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Look at Which components are not supported by S7-PLCSIM V5.4 Best regards, Hristo Mihalev |
Follow us on