(2)| 5/2/2010 9:36 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Dear Sanky, If all the equipment can be reached from one point over several networks, then it must be possible to reach everything. You might place the PG in NETPRO and then do so called routing over several networks. See the next link which equipment could be used for the routing: What are the requirements for using the S7 routing function and which modules can you implement? An example of the routing is shown in the next link: What requirements must be fulfilled and what should I watch out for when executing Routing? Please search further on routing when this is not answering your question. There could also be routing over a SINAUT network, I don't understand your configuration very well. |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on