(0)| 5/25/2010 2:50 PM | |
|
Joined: 12/9/2009 Last visit: 10/30/2025 Posts: 156 Rating:
|
Hello, here you can find a sample programm for S7 communication with FB12 "BSEND" und FB13 "BRECV". http://support.automation.siemens.com/WW/view/en/18516182 With the NCM Diagnostic you can find out whether the S7 connections are established or not. Please check the settings on the parameters of the function blocks FB12 and FB13, for example connection ID, SEND buffer, etc. You have to call the function blocks in both communication partners. On of them has to establish the S7 connection. Good Luck Little Holmes |
Last edited by: little holmes at: 5/25/2010 2:52 PM |
|
Follow us on