(0)| 5/28/2010 10:10 PM | |
|
Posts: 7 Rating:
|
hi all: thanks all Splitted from Probe my HMI program on a PC Online with PLC. |
Last edited by: O_Moderator at: 5/31/2010 8:49 AMnew subject after splitting |
|
| 5/29/2010 6:48 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Let's assume you have some type of panel. There you downloaded WinCC Flex project. First of all you need to take editable version of WinCC Flex project from this panel. (jump this point if you already have it). Is possible to have problem if the transfer of the current project file from the configuration computer to the operating unit wasn't be performed using the Upload option "Enable backtransfer". So, you have WinCC Flex project in your computer. As Darius said also version of WinCC Flex is OK. Open this project with WinCC Flex and change device type to PC station. Now depends what kind of hardware exist on a PC Station (Ethernet, MPI...) you should assign a way to connect to the CPU. For example look at How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet? Take a look aslo at How can you have data from a tag log displayed in table form for panels or the WinCC flexible PC Runtime? This link contains two projects which you could use like examples. Also Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC? Best regards, Hristo Mihalev |
Follow us on