(0)| 9/10/2006 10:38 AM | |
|
Posts: 3149 Rating:
|
Hi have you seen this FAQ?? http://support.automation.siemens.com/WW/view/en/9067116 you could attach your CSV-file in the forum.... nemo |
| 9/11/2006 5:18 AM | |
|
Posts: 87 Rating:
|
Hi Thanx for the reply. Please find the CSV file. AttachmentError while importing from Alarm.csv.zip (522 Downloads) |
| 9/11/2006 10:23 AM | |
|
Posts: 1398 Rating:
|
Your procedure is a little confusing ! 1) The Text Library is used to store texts for alarms and text-type tags. You can import and export the data to and from CSV files using the menus in the Text Library Editor. 2) The Easy Language Tool is used to import / export texts from graphics (i.e. .PDLs). So you should use Easy Language Tool to export all picture texts to a CSV file, edit the CSV file with the Spanish texts and then use the Easy Language Tool to import the CSV file.] Also please read this FAQ -> http://support.automation.siemens.com/WW/view/en/492945 You should not confuse the two! So you cannot export a CSV file from the Text Library and import it into your PDL using the Easy Language Tool. Both editors use different layouts so this is not possible. |
Follow us on