(0)| 5/31/2010 10:28 AM | |
|
Posts: 9 Rating:
|
I've the same problem of PRK, my PCS7 config it's very similar, the only difference is the OS project is in the OS stationand in the ES there is the OS ref. When i try to download the OS I've a error message, in the same point of the PRK log (the project can open, close etc), but the dowload falling at the end. I try also to share the drive C, like someboby suggest in this tread but nothing, PRKyou find a solution ?Thank Splitted from Problem in complete downloading of OS Single station after the first download. |
Last edited by: O_Moderator at: 5/31/2010 1:43 PMnew subject after splitting |
|
Follow us on