(0)| 6/13/2010 10:05 PM | |
|
Posts: 329 Rating:
|
Dear Expert i need to get the pinout connection of db25&db9 with to download and upload master drives paramters via pc or pg? |
| 6/14/2010 8:50 PM | |
|
Posts: 329 Rating:
|
Dear Sir, i think it is possbile and i do my best to findout once i find i will spread here? |
| 6/14/2010 9:04 PM | |
|
Joined: 9/27/2006 Last visit: 1/1/2026 Posts: 12479 Rating:
|
Hello hazem; I think what Umencho actually meant was: what software will you be using this connection, in order to read the drive parameters? -Drive Monitor? -Starter? -another software? thiss way we can tell you what cable/pinout is required to connect with your PC. Hope this helps, Daniel Chartier Edit: for example, look at nhdrives' post in the following thread; he provides links to Drive Monitor software, and an attachment that describes (amngst other things) the cables and connectors needed to use Drive Monitor with Masterdrives: /tf/WW/en/Posts/37036 D.C. |
Last edited by: dchartier at: 6/14/2010 9:16 PMFound link for Drive Monitor settings |
|
| 6/14/2010 9:30 PM | |
|
Posts: 329 Rating:
|
Dear all Depend on the image took from thread cable for communication with simovert drive . i think it will simple now only we will make conversion as follows: from drive side the same for db9 to convert it to db25 db9 db25 pin 2to pin3 pin3 topin2 pin5to pin7 |
| 6/15/2010 5:59 AM | |
|
Joined: 3/21/2006 Last visit: 12/31/2025 Posts: 10244 Rating:
|
Hello, Yes, you are right. If you want to use the example with a DB25, simply replace the pin numbers of the connector according to the conversion table below in attachment. Best regards, Hristo Mihalev |
| 6/15/2010 11:37 AM | |
|
Posts: 329 Rating:
|
Dear all , ther was wrong in connection for db9 with drive side. here are you the right attached one |
This contribution was helpful to
|
|
| 6/18/2010 7:37 PM | |
|
Posts: 329 Rating:
|
Dear All, The final attached cable for db25 will be as attached now and as i told before there is wrong in db9 which i took from another forum so i illustrated this point and here are you the both db9&db25 |
Follow us on