6/29/2010 8:14 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
PCS7 7.1 sp1. Is it just me or is changing the symbollist a pain in the *ss.. Example: I have a signal at Q130.0 called: spare. I want to change it to... i dunno "Activate unit". 1. Open symbollist in Simatic 2. Change name and save 3. In CFC click on options and click Update with symbol table 3. Compile CFC charts When compiling the CFC, I always get an error: "Key not found". When I try to compile it a second time, it works but if I have a CH_DO connected to Q130.0 with the original name: "spare", the compiler gives me an error because the name is not recognized. I have to delete the signal and interconnect it again. Now the name is changed from "spare" to "Activate unit" and then its ok... This doesn't work like a charm... Is it because i'm doing something wrong? or is it a common problem? Grtz |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on