7/5/2010 2:28 PM | |
Joined: 4/29/2009 Last visit: 11/12/2023 Posts: 4 Rating:
|
Sorry if I disturb but I have see the post and I have a similar prolem. I use PCS7 6.1 sp3 , in the project I have 15 Multiclient and 6 Server ( 3 couple of rendundant server) In one couples OSServer3 need onlone user have possibility to process controlling ,and one user for higher process controllig , the user of othe OSserver1 e 2 need only visualizzation in OSServer 3 I have configure manualy the user administartion rigth , I not have the picture inside plant view the picture is only in WinCC , I have manualy make picture tree manager hierarchy. In the OSServer3 all is good only user atorizated have possibility to operate. In other OSServer 1 and 2 have strange think , in same picture 2 PID Control assigned in the same OS in one I have possibilit to Operate in Othe NO , please help me best regards and thanks Splitted from problem with user level areas PCS7. |
Last edited by: O_Moderator at: 7/6/2010 8:56 AMnew subject after splitting |
|
Follow us on