(0)| 7/21/2010 1:40 PM | |
|
Posts: 2 Rating:
|
Good day. I am one of the lucky ones " sometimes I don't feel so lucky" to work with the package called CIS_CK v8.05.03. We are currently using the exclusive control within our split SCADA interface, but the one thing thatI came across during some testing is that the block used "EXCL_OP FB699" has got no effect on the CIS_CK faceplates forBIN_IN (FB862) and MEAS (FB665). I have tried to post under the SESAM forums https://sesam.erlm.siemens.de/sesam/sesamservlet?cmd=TrustToolPage&tool=CIS+Control+Kernelbut form some reason only moderators are allowed to post there. Any input will be greatly appreciated. |
Follow us on