(0)| 8/2/2010 9:26 AM | |
|
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, wich flexible version do you use and how many functions do you have projected at one button? best regards |
| 8/4/2010 7:27 AM | |
|
Joined: 9/28/2005 Last visit: 12/9/2025 Posts: 2957 Rating:
|
Hello, Its very hard to find problem from information you provided. The best would be to get the project, but if this is not possible then remove functions from button one by one and see when situation will be better. By using that method you will find at least function whuich causes the problem. Then you can inspect source code of the function and check what is wrong with it. Also check the limitations of the panel here http://support.automation.siemens.com/WW/view/en/19169911/td. It is "micro" panel so it has a lot of limitations. You should check if you not overcome any restrictions. |
Last edited by: Darius at: 8/4/2010 7:29 AMBest regards, |
|
Follow us on