(0)| 8/5/2010 8:43 AM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Dear Bavarian335i, I guess you have seen this link: Which settings must you make on the RT loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC? Are both versions equal? (Including any Servicepacks) Best regards, Wizard |
| 8/5/2010 4:08 PM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Hi, Perhaps the following link, might help: how do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300/S7-400 via industrial ethernet? Best regards, Wizard |
| 8/6/2010 5:12 AM | |
|
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Hi, |
| 8/7/2010 4:16 AM | |
|
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Bavarian, I had the same problem three weeks ago. The PC was communicating fine and suddenly stopped communicating. I could ping the PLC but no communication. I ended up removing the Wincc Flex Run-time and re-installing it. I set the PG/PC interface and it was good to go. How about using NCM Diagnostics which should be installed on your PC for diagnosing the communication issue. Take a look at the attached file. Regards, Behnam www.sigmaprocess.ca |
Last edited by: Behnam R at: 8/7/2010 4:18 AM |
|
Follow us on