8/11/2010 12:15 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, S7 Basic Communication which is supported from all S7-300/400 CPUs is generally suitable for the transmission of small data volumes via non-configured S7 connections. The problems there are limitted quantity of data and distance between both partners. Take a look at Options for communications via MPI . Give more details... Best regards, Hristo Mihalev |
8/11/2010 1:58 PM | |
Posts: 73 Rating:
|
Dear sir, |
This contribution was helpful to
1 thankful Users |
Follow us on