(1)| 10/5/2006 3:15 PM | |
|
Posts: 70 Rating:
|
The other fields are all the parameters and checkboxes configured in the tag definition dialog, such as the linear scaling parameters and startup/fallback value of the tag. The best way to find out what you need for the tags you are importing is tocreate a dummyinternal tag of each tag type you need to import, then export all these tags. This will give you the correct formats of parameters for your tags. You probably then mainlyneed the "Spec" column, which is usually the actual PLC address of the tag, eg: "DB100,DBB0". Try changing parameters in the tag dialog and expoorting again - this will show how each property is set in the export file. Columns like "Flag" are bit maps -certain options switch certain bits on or off. Alternatively, have you tried the Excel Configuration tool? This is similar toExIm but lets you use Excel directly to edit the tag database. You can install it from the WinCC v6 installation CD in the "Options" section. |
| 10/6/2006 11:18 AM | |
|
Posts: 5 Rating:
|
ok, thank you I will do it like that... |
Follow us on