(0)| 8/24/2010 5:42 AM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Are you comissioning new crane ?? Or you are facing problem in existing one?? I think you should perform Auto Tunning again. You mentioned that you are using two motors. Are they for same purpose?? I mean both motors are used for Hoist/Lower Purpose? Are they running in Parallel? If yes, you should not use Vector Control in such case.. If NO, Please Perform Autotunning as I said. Also check operation with Load Decoupled (Only Motor Connected) Also check Encoder Feedback. You wrote that you already checked but most of the time fault is in Encoder Feedback. Check my following Post and check your encoder Feedback as suggested in that.. Trouble shooting in Vector Control Mode I hope this will Help Best Regards, Devesh Vithani |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on