(0)| 10/12/2010 1:04 PM | |
|
Posts: 11 Rating:
|
Hey all, I have a problem using the step 5 software on my PC. I cannot open the "Cross-Reference" or "Program Structure"under "Documentation". Neither can I perform a compare. When I open for example "Program Structure" I can select the options like which program file, output to screen etc.. but when I press "output" then I get the error message: Cannot load application I found already this link: Cannot Load Application Error Message (Entry ID: 11376026 ) In that link their is described what to do but after trying these things it's still is not working. Everything fits like in that link. The OS, version of Step 5 and the parts that don't work. So if any off you had the same problem or know something else I can try, pls let me know. I also tried checking my account settings but those seem ok also. Below the details of my PC. Microsoft Windows XP pro version 2002 Service Pack 3 CPU Core2Duo T7800 @2.60GHz 3.00GB RAM Simatic S5 Step 5 / ST Version 7.17 (Date 12.02.01) |
Last edited by: Kib0sh at: 10/12/2010 1:10 PMLink didn''t work. Last edited by: Kib0sh at: 10/12/2010 1:09 PMLast edited by: Kib0sh at: 10/12/2010 1:07 PMLast edited by: Kib0sh at: 10/12/2010 1:06 PM |
|
Follow us on