(0)| 10/15/2010 9:34 AM | |
|
Joined: 10/9/2007 Last visit: 1/21/2026 Posts: 1295 Rating:
|
Hi gre_m May PCS7 work also separate from WinCC? one or more computers for PCS7 and WinCC as independent computers? Does it improve performance? Mike J Splitted from what is the difference between S7 and PCS7 "hardware and software"?. |
Last edited by: O_Moderator at: 10/15/2010 11:33 AMnew subject after splitting Energy Automation products: Sicam, Siprotec, Digsi |
|
| 10/15/2010 2:15 PM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello Mike; PCS 7 is an integrated hardware and software package, but as far as deployment it can be setup in many ways. For the small projects, you can have a single PC used as a PLC and SCADA programmer. Generally, for a medium to large project, you would set it us as a multiproject, which means that different computers will be used for different parts of the project: the ES (engineering station) will use one (or more) computer for the programming of the PLCs logic; the OS (operating stations) will often be distributed in a server/client constellation (multiserver/multiclient applications are common in large plants). You can have dedicated alarm servers, maintenance PCs... as you need them. Have a look at the link I proposed in the earlier thread so you can have more details: https://eb.automation.siemens.com/goos/catalog/Pages/ProductData.aspx?catalogRegion=WW&language=en&nodeid=5309999&tree=CatalogTree®ionUrl=%2f#activetab=product Hope this helps, Daniel Chartier |
Follow us on