11/19/2010 5:43 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Like Routing among PROFIBUS subnets on one CPU 400 using the DriveMonitor of DriveES and What should I do if I have set my PG/PC interface to ISO-Industrial Ethernet so I can use Routing with Starter and DriveES to access MICROMASTERS on Profibus from the network port on my PG or PC and I find that the communication doesn't work? Best regards, Hristo Mihalev |
Follow us on