(0)| 1/12/2011 5:47 PM | |
|
Posts: 2964 Rating:
|
Hi.... Is this a newly commissioned machine ? all of a sudden are you getting this error? If i understand corectly your error messgae is "waiting for first thread cut" normally with the DC motor you will not have a proper thread formation your using only external encoder that is only for position where as motor is not having the encoder for colsed loop veloctiy... Forming the thread on your case will be difficult....Check it out nothing is impossible Can you try changing 32110 $MA_ENC_FEEDBACK_POL[0,AX1]=1 'to -1 and check? >FFWON and SOFT was used in the part program>The setting data 42010 [0],[1] = 0 >Dynamic match was enabled in the axis MD 32900=1 for the interpolating axis > Auto optimize the axis... > optimize the accelearion parameters 32300 Attaching youthe link of 802D SL https://www.automation.siemens.com/doconweb/content.asp?item=11192&cd=sinumerik_sinamics_04_2010_e&scope=all Regards, Ekalavya |
Follow us on