(0)| 11/8/2006 9:43 PM | |
|
Posts: 2 Rating:
|
Hello, After reviewing the Sm@rtAccess Documentation on catalog ST 80 -2006 (section 4), I still could not figure out whether if Sm@rtAccess enables monitoring of a remote PC running WinCC Flexible runtime, from another PC running WinCC Flexible runtime as well. To clarify: My customer has a PC running WinCC Flexible runtime on the field as its HMI/SCADA solution for a Simatic Application. My customer wishes to monitor some operation parameters from a distance by using Sm@rtAccess to connect its local PC (Having WinCC Flexible Runtime) with the one on the field (which also has WinCCFlexible installed) using a single Sm@rtAccess license. Diagrams on catalog show as if only a PC running WinCC Flexible runtime could remotely access HMI devices as TPs, OPS or MPs through Sm@rtAccess. Please advice if this application is feasible, and if not, please suggest a software application that could enable a remote PC to access a PC Station using WinCC Flexible runtime. Hope I have made myself clear, thank you. |
| 11/9/2006 4:35 PM | |
|
Posts: 3149 Rating:
|
Hi, perhaps the Getting-Started can give you some info?? http://support.automation.siemens.com/WW/view/en/18657078 nemo |
| 11/10/2006 12:52 PM | |
|
Posts: 317 Rating:
|
Hi Hernandez. Just to add to Nemo's advice. In WinCC Flexible you have a control in the toolbox called 'Sm@rtclient view'. Youembed this in a screen anduse it to view the 'target' HMI application. Hope this helps. |
Follow us on